Take this example of two homeowners – Sophie and Marc – who each renovated their homes in Lyon, France, in 2015.
Heat pump and boiler installation costs
Sophie invested in an air-to-water heat pump, while Marc opted for a modern condensing gas boiler.
There are many different types of heat pumps, so the cost of buying and installing can vary significantly, from around €9,200 to around €20,800. There could be additional costs to consider if you decide to carry out other improvements, such as changing existing emitters, or installing insulation.
Gas boilers are generally cheaper to install, ranging from €3,000 to €6,000.
Depending on where you live though, you might be able to get a grant towards the cost of a heat pump. You can read more about incentive schemes in your area here.
The same was true for Sophie. While her installation cost was high compared to Marc’s gas boiler, she was able to offset this using a government grant.
What are the maintenance costs and lifespan
Another factor in the return on investment equation is how long your heating system will last and how much it costs to maintain and run during that time.
If looked after properly, a heat pump can last 15 to 20 years. Maintenance involves routine checks and cleaning, and typically costs around €115 to €230 per year.
Due to their combustion processes, gas boilers require careful maintenance and servicing, which can cost between €115 and €350 per year. Their average lifespan is 10 to 15 years.
Ten years after installing their new heating systems, Marc’s gas boiler is now nearing the end of its life, while Sophie can expect to get another 5 to 10 years from her heat pump.
Sophie’s maintenance costs have been low, while Marc has experienced higher maintenance costs for his gas boiler.
Energy prices and running costs
A heat pump draws up to 75% of its energy from nature for free, with the remainder powered by electricity, while a boiler relies entirely on gas. The comparative running costs therefore depend on the cost of household electricity versus gas.
Particularly in recent years, we’ve seen significant price fluctuations in natural gas, due to geopolitical tensions, market demand and supply chain disruptions. Seasonal and geographical factors also play a part and gas prices may spike during harsh winters.
While modern heat pumps can operate effectively even in colder temperatures, electricity prices can also be affected by factors such as generation costs and government policies.
It’s therefore difficult to predict exactly what will happen with energy prices, but over the last 10 years, Sophie has also installed photovoltaic solar panels to reduce her dependence on electricity prices. Once the installation and maintenance costs of these panels are factored in, she has still seen a reduction in her net electricity bills for this specific installation, while Marc’s running costs have been variable and sensitive to fluctuating gas prices.